This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ubi file system creation issue for custom am335x board



Hi, there

In the case of using arago-base-tisdk-image-am335x-evm.ubi as rootfs the board works well, it can get into bash promt. But when I tried to create the ubi image using commands of mkfs.ubifs –F -q -r /home/usr/fs -m 2048 -e 126976 -c 2047 -o ubifs.img and ubinize -o ubi.img -m 2048 -p 128KiB ubinize.cfg(/home/usr/fs is the location of file system unzipped from arago-base-tisdk-image-am335x-evm.tar.gz), this ubi image seems not working. I have attached the kernel log for reference. Any suggestion about this?

[ 2.241607] UBI: attaching mtd9 to ubi0
[ 2.817959] UBI: scanning is finished
[ 2.841403] UBI: volume 0 ("rootfs") re-sized from 826 to 920 LEBs
[ 2.849105] UBI: attached mtd9 (name "NAND.file-system", size 118 MiB) to ubi0
[ 2.856704] UBI: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[ 2.863872] UBI: min./max. I/O unit sizes: 2048/2048, sub-page size 512
[ 2.870832] UBI: VID header offset: 2048 (aligned 2048), data offset: 4096
[ 2.878051] UBI: good PEBs: 944, bad PEBs: 0, corrupted PEBs: 0
[ 2.884278] UBI: user volume: 1, internal volumes: 1, max. volumes count: 128
[ 2.891784] UBI: max/mean erase counter: 1/0, WL threshold: 4096, image sequence number: 1971850362
[ 2.901313] UBI: available PEBs: 0, total reserved PEBs: 944, PEBs reserved for bad PEB handling: 20
[ 2.910961] UBI: background thread "ubi_bgt0d" started, PID 853
[ 2.998384] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 3.004804] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 3.029331] libphy: 4a101000.mdio: probed
[ 3.033554] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Atheros 8031 ethernet
[ 3.059373] cpsw 4a100000.ethernet: Detected MACID = d0:ff:50:03:da:96
[ 3.080274] input: volume_keys.8 as /devices/volume_keys.8/input/input1
[ 3.098925] omap_rtc 44e3e000.rtc: setting system clock to 2015-02-11 16:09:32 UTC (1423670972)
[ 3.111291] ALSA device list:
[ 3.114429] No soundcards found.
[ 3.138526] UBIFS: background thread "ubifs_bgt0_0" started, PID 867
[ 3.270025] UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[ 3.276355] UBIFS: LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes
[ 3.286001] UBIFS: FS size: 115421184 bytes (110 MiB, 909 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs)
[ 3.296336] UBIFS: reserved for root: 0 bytes (0 KiB)
[ 3.301681] UBIFS: media format: w4/r0 (latest is w4/r0), UUID 4223E53A-8A3C-4B0D-A941-1EF21870489D, small LPT model
[ 3.351088] VFS: Mounted root (ubifs filesystem) on device 0:14.
[ 3.369489] devtmpfs: mounted
[ 3.372968] Freeing unused kernel memory: 268K (c07be000 - c0801000)
[ 3.396318] Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

Best Regards

Yang