Hi,
I am working on TMS320C6A8167 ARM Cortex A8 processor. I have booted the processor with the Linux Kernel and want to know if I can display the kernel on my PC running Ubuntu 14.04. If so, how to do it?
Working on CCSv5.5.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am working on TMS320C6A8167 ARM Cortex A8 processor. I have booted the processor with the Linux Kernel and want to know if I can display the kernel on my PC running Ubuntu 14.04. If so, how to do it?
Working on CCSv5.5.
Thanks
One thing you should modify for sure is the ti-ezsdk_dm816x-evm_5_05_02_00/bin/setup-host-check.sh script, called from the ti-ezsdk_dm816x-evm_5_05_02_00/setup.sh script.
In the setup-host-check.sh script, only Ubuntu 10.04 LTS, Ubuntu 11.10 and Ubuntu 12.04 is supported. You should add Ubuntu 14 support there, if not the setup.sh script will fail.
Regards,
Pavel
Hi,
Sorry to bother again but I installed the EZSDK
Ran the setup.sh
Started minicom and loaded the script that was made by setup.sh (setup_uimage-tftp_fs-nfs.minicom)
I have connected the board with a USB as well as UART cable but I do not see anything happening i.e. no linux bootup or matrix load.
What am I doing wrong?
Thanks
Raunak
Raunak Kalani said:and loaded the script that was made by setup.sh (setup_uimage-tftp_fs-nfs.minicom)
I am using picocom, and I am not using this script (made by the setup.sh).
host$ sudo picocom -b 115200 /dev/ttyUSB0 --send-cmd "sx -vv"
picocom v1.4
port is : /dev/ttyUSB0
flowcontrol : none
baudrate is : 115200
parity is : none
databits are : 8
escape is : C-a
noinit is : no
noreset is : no
nolock is : no
send_cmd is : sx -vv
receive_cmd is : rz -vv
Terminal ready
When you plug UART-to-USB cable in the USB port of the host machine (Ubuntu PC), you should see /dev/ttyUSBx (in my case /dev/ttyUSB0). Then you pass this as a parameter to the picocom.
Do you have the same output as me in your linux terminal (Applications -> Accessories -> Terminal)?
BR
Pavel
Raunak,
Raunak Kalani said:raunak@ubuntu:~$ sudo picocom -b 115200 /dev/ttyUSB0 --send-cmd"sx-vv"
This is not correct, as you do not have space between --send-cmd and "sx -vv".
You have: --send-cmd"sx -vv"
It should be: --send-cmd "sx -vv"
Raunak Kalani said:After this It asks for login .
How should I login
Can you try without sudo command?
raunak@ubuntu:~$ picocom -b 115200 /dev/ttyUSB0 --send-cmd "sx-vv"
BR
Pavel
Hi,
I tried without sudo then also login as root failed.
baudrate is : 115200
parity is : none
databits are : 8
escape is : C-a
local echo is : no
noinit is : no
noreset is : no
nolock is : no
send_cmd is : sx-vv
receive_cmd is : rz -vv
imap is :
omap is :
emap is : crcrlf,delbs,
Terminal ready
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org tmdxscbp6618x ttyO0
Arago 2011.06 tmdxscbp6618x ttyO0
tmdxscbp6618x login: root
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org tmdxscbp6618x ttyO0
Arago 2011.06 tmdxscbp6618x ttyO0
tmdxscbp6618x login: root
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org tmdxscbp6618x ttyO0
Arago 2011.06 tmdxscbp6618x ttyO0
tmdxscbp6618x login:
Any way to change password?
Thanks
Raunak
Can you provide me your boot arguments? Are you loading your rootfs from ethernet/EMAC?
Do you have the below folder on your Ubuntu PC?
/home/users/raunak/targetfs/home/root/
BR
Pavel
I have the folder /home/raunak/targetfs/home/root where i have made another folder dm816x and placed the helloworld executable there.
what is rootfs?
My steps:
run picocom -b 115200 /dev/ttyUSB0 --send-cmd"sx-vv"in the terminal
give root as login password
follow the steps in the above site
I do not have ethernet connection to the SCBP board.
P.S. the board was loaded with Arago build with
U-Boot binary:
u-boot-tmdxscbp6618x-git-r0.0.noxip.bin
Kernal binary:
uImage-2.6.37-r0-r0rtmdxscbp6618x.bin
Thanks
Raunak
Raunak,
Raunak Kalani said:I have the folder /home/raunak/targetfs/home/root where i have made another folder dm816x and placed the helloworld executable there
Can you try to place the executable in /home/raunak/targetfs/home/root/ or in /home/raunak/targetfs/home/. Is there any difference?
Raunak Kalani said:what is rootfs?
rootfs means root filesystem, the filesystem used with the linux kernel.
Raunak Kalani said:My steps:
run picocom -b 115200 /dev/ttyUSB0 --send-cmd"sx-vv"in the terminal
give root as login password
Can you provide me full console output log?
Raunak Kalani said:I do not have ethernet connection to the SCBP board
These steps are valid when you have ethernet connection between host (Ubuntu PC) and target (C6 Intergra board).
Regards,
Pavel
raunak@ubuntu:~$ picocom -b 115200 /dev/ttyUSB0 --send-cmd "sx-vv"
picocom v1.7
port is : /dev/ttyUSB0
flowcontrol : none
baudrate is : 115200
parity is : none
databits are : 8
escape is : C-a
local echo is : no
noinit is : no
noreset is : no
nolock is : no
send_cmd is : sx-vv
receive_cmd is : rz -vv
imap is :
omap is :
emap is : crcrlf,delbs,
Terminal ready
at 0x005178c0: read 0xd8a374fe,
U-Boot 2010.06 (Oct 26 2011 - 15:33:11)
TI8168-GP rev 1.1
ARM clk: 987MHz
DDR clk: 398MHz
DRAM: 2 GiB
NAND: HW ECC Hamming Code selected
256 MiB
###### ###### ######## ########
## ## ## ## ## ## ## ##
## ## ## ## ## ##
###### ## ######## ########
## ## ## ## ##
## ## ## ## ## ## ##
###### ###### ######## ##
Net: Detected MACID:d4:94:a1:a6:5:6c
DaVinci EMAC
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x280000, size 0x440000
4456448 bytes read: OK
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Arago/2.6.37-r0/tmdxscbp6618x
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2068588 Bytes = 2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (a0868396@gta0868396-ubuntu10) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Thu Sep 29 17:38:36 EDT 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: tmdxscbp6618x
bootconsole [earlycon0] enabled
reserved size = 0 at 0
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 1.1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttyO0,115200n8 root=/dev/mtdblock3 rootfstype=jffs2 rw noinitrd earlyprintk mem=512m mtdparts=omap2-nand.0:2432k(uboot)ro,128k(params)ro,4352k(kernel),204928k(filesystem),-(reserved)
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 512MB = 512MB total
Memory: 515332k/515332k available, 8956k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xe0800000 - 0xf8000000 ( 376 MB)
lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0035000 ( 180 kB)
.text : 0xc0035000 - 0xc03e5000 (3776 kB)
.data : 0xc03e6000 - 0xc041cec0 ( 220 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQpt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_mux_init: Add partition: #1: core, flags: 0
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
NET: Registered protocol family 2
IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP reno registered hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
Raunak,
Raunak Kalani said:Kernel command line: console=ttyO0,115200n8 root=/dev/mtdblock3 rootfstype=jffs2 rw noinitrd earlyprintk mem=512m mtdparts=omap2-nand.0:2432k(uboot)ro,128k(params)ro,4352k(kernel),204928k(filesystem),-(reserved)
You are booting your board from NAND flash, it seems your board come with already flashed NAND chip. In order to be able to execute your application, you should place/flash it in NAND. The NAND filesystem come from ti-ezsdk_dm816x-evm_5_05_02_00/filesystem/arago-base-tisdk-image-dm816x-evm.tar.gz. You should untar this file, place your executable and then transform this folder into JFFS2 or UBIFS format for flash it into NAND. This is not an easy task.
C6A device can boot from: SD card, Network/Ethernet, NAND, SPI, NOR
I would recommend you to try first with SD card. You need SD card reader connected to your host (Ubuntu PC) through USB cable. You should plug SD card into the card reader and follow the instructions from ti-ezsdk_dm816x-evm_5_05_02_00/docs/DM816x_EZ_Software_Developers_Guide.pdf, 6.7 How to create an SD card. The mksdboot.sh script will create two partitions in your SD card, BOOT and ROOTFS. BOOT partition/folder will contain the pre-built u-boot and linux kernel from the ti-ezsdk_dm816x-evm_5_05_02_00/board-support/prebuilt-images/ folder. ROOTFS partition/folder will contain your filesystem which is based on ti-ezsdk_dm816x-evm_5_05_02_00/filesystem/ezsdk-dm816x-evm-rootfs.tar.gz.
After mksdboot.sh script finished, you just need to place your executable in the /ROOTFS/home/root/ folder. Then remove the SD card from the PC, place it in the target board, configure the boot pins for SD boot and power on the board.
BR
Pavel
Thanks Pavel I was able to get the file over tftp server and run it on the board using tftp -g -r helloworld 192.168.1.1 69 from tftpboot folder.
Raunak
Hi Pavel
I am trying to run the whole thing in windows as well and want a arm compiler for the platform. Can you share the link for a .exe file.
Thanks
Raunak