Hi,
I encoded a sequence using your HEVC encoder running on an octal DSP card. The HEVC encoder version used is C66x_h265venc_02_00_00_02_ELF. I have used the scripts provided within the MCSDK Video 2.2.0.45, with the following encoder config file 4848.LowDelay_codecParams1080p60.cfg. The encoded sequence (using 4 DSP's) is blue_sky_1080p25.123.
When using a third party decoder, single threaded decoding works fine but wavefront parallel decoding (using libde265) results in severe visual artefacts. These artefacts appear to be due to incorrect entry point offsets for WPP. Using the same decoder in combination with other encoders (e.g., x265) with WPP enabled results in no issues, which suggests that this an issue at the encoder side.
Best regards,
Jurgen