I have a OMAP35x EVM2 board with us.I am trying to flash the XLDR,EBOOT using EVM Flash tool over UART. It is always giving 'Failed to Connect to target'.
I had tried in both Windows 7 & Windows Vista PC.But with Windows XP PC it is working fine.
Could anyone tell me what i am missing?
Download [12:40:29]: [00] dl.cpp ( 143): Thread 0x00001948 created in DLSession::init() with thread function dl_msg_handler()
Download [12:40:29]: [00] dl.cpp ( 936): State Change --> New state: Disconnected
Download [12:41:12]: [00] dl.cpp ( 959): Recieved primitive in state Disconnected APP(ThreadId 0x1430)-> DL(ThreadId 0x1948): DL_CONNECT_REQ
Download [12:41:12]: [00] dl_connecting.cpp ( 676): State Change --> New state: Connecting
Download [12:41:12]: [00] dl_connecting.cpp ( 572): State Change --> New state: ConnectingPBP
Download [12:41:12]: [00] dl_connecting.cpp ( 596): Thread 0x000018F4 created in DLConnectingClass::dl_flashing_mode_connect() with thread function dl_connect_handler()
Download [12:41:12]: [00] dl_connecting.cpp ( 598): Waiting for connect thread to copy data from primitive...
Download [12:41:12]: [00] dl_connecting.cpp (1022): Initiating OMAP ROM code communication
Download [12:41:12]: [00] dl_connecting.cpp (1026): State Change --> New state: ConnectingPBPSignalling
Download [12:41:12]: [00] dl_connecting.cpp (1039): Opening UART/USB connection
Download [12:41:12]: [00] dl.cpp ( 601): Freeing primitive: DL_CONNECT_REQ
Download [12:41:12]: [00] dl_connecting.cpp ( 152): Sending primitive: DL(ThreadId 0x18F4)-> APP(ThreadId 0x9C4): DL_RESET_IND
Download [12:41:12]: [00] dl_connecting.cpp ( 153): Waiting for target to reset
Download [12:41:19]: [00] dl_connecting.cpp (1103): Unable to read ASIC ID. Searched 32 bytes of data and did not find start of ASIC ID
Download [12:41:19]: [00] dl_connecting.cpp ( 768): Releasing UART/USB connection...
Download [12:41:19]: [00] dl_connecting.cpp ( 783): Error occurred during ROM-code connect phase, return code 0xFFFFFFFE
Download [12:41:19]: [00] dl_connecting.cpp ( 789): State Change --> New state: Disconnected
Download [12:41:19]: [00] dl_disconnected.cpp ( 49): Dl connect operation failed. Error code: 0xFFFFFFFE
Download [12:41:19]: [00] dl_disconnected.cpp ( 51): Sending primitive: DL(ThreadId 0x18F4)-> APP(ThreadId 0x9C4): DL_CONNECT_CNF