Hello!
Can you advise, which h264 encoder parameters should be adjusted to increase encoding speed, please?
I'm using DM368 at 432MHz core and 340MHz DDR, and when encoding video 1980 x 1088, function
VIDENC1_process (processing buffer with frame) takes not less then 43ms, i.e. my speed is below 25fps.
Encoder is ver. 2.30.00.04. My settings are 2Mbps bit rate, encodingPreset = XDM_HIGH_SPEED, input chroma 420SP,
Frame rate 25fps, others are default.
What should I change at first order to get at least 25 fps?