This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issues porting Audio example from PSP 1.30

When I try to run the audio example, after importing it to CCS 6 using the Import legacy project option I get the following error?

"C:/ti/pspdrivers_01_30_00_05/packages/ti/pspiom/examples/evmOMAPL137/audio/src/audioSample_main.c", line 57: fatal error #5: could not open source file "Audio.h"

I have installed psp 1.30 in a different location than the suggested by the executable. Is there a environment variable I need to add or modify? Manually adding the header is not an easy option since, after adding Audio.h there are like 20 more headers required. 

I also will need to add the edmav3 enviroment variable for proper linking. 

Any help or guidance will be greatly appreciated. I'm using a EVMOMAPL-137.