This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using I2C0 bus of AM3358 for HDMI DDC Bus...

Other Parts Discussed in Thread: AM3358, TPD12S016

I am having difficulty reading HDMI monitor EDID  using read-edid v3.02 in linux.  Command line prompt response from ARM is No EDID on Bus 0 & No EDID on Bus1...    I am using I2C0 Bus of AM3358 which has 3.3K PUs connected to HDMI connector 'DDC bus' via a TPD12S016, TI HDMI companion chip with I2C level shifting.  from 3.3V to 5V.  The I2C bus going into TPD12S016 without HDMI connection to monitor looks okay but as soon as I hook HDMI cable from monitor to board the ACK line is not able to drive completely high.  These are only devices connected in I2C0 bus path from ARM!!!

Thanks,

James