This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help!!! Jpeg encode crashed on DM6446!!

Other Parts Discussed in Thread: CCSTUDIO

Hi, I meet a problem when I use Jpeg library( Build ID: 2.00.002) in my project.

My code is bellow which very simple, I do it as the demo from “dm6446_jpegenc_2_00_002_production\packages\ti\sdo\codecs\jpegenc\app\Client\Test”.

 

-When I run this task in DSP side without DSPlink environment, the .out file is loaded via emulator from JTAG, the While-loop can run continuously.

-But When I run this task in DSP side with DSPLINK, which means boot from arm and two cores run together, the program crashed after soon. I doubted that maybe the DSPLINK configuration is incorrect on my project. Then I used the dsplink demo from “dsplink_1_30_08_02\packages\dsplink\dsp\src\samples\scale”. I add my code in the function “static Int tskScale()” , before the DSPLINK related code” status2 = TSKSCALE_create (&info);”. It crashed as well. Of course, I have checked the stack size and heap size, and enlarge it if it’s too small. Besides, I know the program crashed in "IIMGENC1fxns->process" by invoking the “abort()” function.

 

/*********************************************************************************/

 

#define CIF_HEIGHT 288

#define CIF_HALF_HEIGHT 144

#define CIF_WIDTH 352

#define CIF_IMG_SIZE  101376 //(CIF_HEIGHT * CIF_WIDTH)

#define CIF_HALF_SIZE 50688

#define CIF_YUV420_SIZE  152064 // 10

 

JpegProc()

{

 

        FILE *pFileIn;

        int swRtnVal;   

        UINT8 *pInBuf[3];

        Uns uwCnt = 0;

   

        int  uwImgLength = 0;        

        IIMGENC1_Params tGlobalParams;

        IIMGENC1_DynamicParams tDynamicParams;        

        IALG_Handle handle;

 

        IIMGENC1_Fxns            *IIMGENC1fxns;

        IIMGENC1_Status          status;

        XDAS_Int32   retVal;

  

        /* Input/Output Buffer Descriptor variables */

        XDM1_BufDesc inputBufDesc, outputBufDesc;

 

        IIMGENC1_InArgs          inArgs;

        IIMGENC1_OutArgs         outArgs;

       

        int ii;

        int swAuNum;  

 

         pFileIn = fopen("C:\\CCStudio_v3.3\\MyProjects\\Data\\yuv420_uvuv.yuv","rb");

         if (pFileIn != NULL)

         {

             swRtnVal = fread(uacImgYUV,1,CIF_IMG_SIZE,pFileIn);

             if (swRtnVal != CIF_IMG_SIZE)

             {   

                 LOG_printf(&trace, "fread failed 1 %d\n",swRtnVal );

     

             }   

         }

         else

         {

               LOG_printf(&trace, "fopen failed\n" );     

         }

        

        pInBuf[0] =  uacImgYUV;

 

         tGlobalParams.size = sizeof(IIMGENC1_Params);

         tGlobalParams.maxHeight =288;

         tGlobalParams.maxWidth = 352;

         tGlobalParams.maxScans = 0;

         tGlobalParams.dataEndianness  = XDM_BYTE;

         tGlobalParams.forceChromaFormat = XDM_GRAY;//XDM_YUV_420P;  

 

 

        if ((handle =  (IALG_Handle)ALG_create (

              (IALG_Fxns *) &DMJPGE_TIGEM_IDMJPGE,

              (IALG_Handle) NULL,

              (IALG_Params *) &tGlobalParams)) == NULL)

        {

        #ifdef DEBUG_INFO_PRINT

             LOG_printf(&trace, "\nFailed to Create Instance... Exiting for this configuration..");

        #endif

       return  FAILURE;

        }

 

        status.size                     = sizeof(IIMGENC1_Status);   

          inArgs.size                     = sizeof(IIMGENC1_InArgs);

          outArgs.size                    = sizeof(IIMGENC1_OutArgs);

          outArgs.extendedError           = 0;

          outArgs.bytesGenerated          = 0;

          outArgs.currentAU               = 0;

 

         tDynamicParams.captureWidth = 352;

         tDynamicParams.generateHeader = 0;

         tDynamicParams.inputChromaFormat = XDM_GRAY;//XDM_YUV_420P;

         tDynamicParams.inputHeight = 288;

         tDynamicParams.inputWidth = 352;

 

         tDynamicParams.numAU = 0;

         tDynamicParams.qValue = 80;

         tDynamicParams.size = sizeof(IIMGENC1_DynamicParams);  

 

 

        while(1)

        {

            /* Activate the Algorithm   */

            handle->fxns->algActivate(handle);

 

            /* Assigning Algorithm handle fxns field to IIMGdecfxns */

            IIMGENC1fxns = (IIMGENC1_Fxns *)handle->fxns ;

 

            /* Optional: Set Run time parameters in the Algorithm via control()*/       

            retVal = IIMGENC1fxns->control((IIMGENC1_Handle)handle, XDM_SETPARAMS,

                                            (IIMGENC1_DynamicParams *)&tDynamicParams,

                                            (IIMGENC1_Status *)&status);

            if(retVal != IALG_EOK || status.extendedError)

            {

               

                LOG_printf(&trace, "control failed(%d)",status.extendedError);

                return  FAILURE;

           

            }

           

             /* Get Buffer information */   

            retVal =  IIMGENC1fxns->control((IIMGENC1_Handle)handle,

                                  XDM_GETBUFINFO,

                                  (IIMGENC1_DynamicParams *)&tDynamicParams,

                                  (IIMGENC1_Status *)&status);

             if(retVal != IALG_EOK || status.extendedError)

             {

                LOG_printf(&trace, "control failed(%d)",status.extendedError); 

                return  FAILURE;

            

             }

            

             swAuNum = status.totalAU;

            

             /*Fill up the buffers as required by algorithm                            */

             inputBufDesc.numBufs  = status.bufInfo.minNumInBufs ;

             inputBufDesc.descs[0].buf     = (XDAS_Int8 *)pInBuf[0];

             inputBufDesc.descs[0].bufSize = status.bufInfo.minInBufSize[0];

 

             for(ii=0; ii< (status.bufInfo.minNumInBufs - 1);ii++ )

             {

               inputBufDesc.descs[ii+1].buf = (XDAS_Int8 *)pInBuf[ii + 1];

               inputBufDesc.descs[ii +1].bufSize =

                 status.bufInfo.minInBufSize[ii +1];

             }

            

             outputBufDesc.numBufs     = status.bufInfo.minNumOutBufs ;

             outputBufDesc.descs[0].buf     =(XDAS_Int8 *) uacImgOutput;

             outputBufDesc.descs[0].bufSize = CIF_YUV420_SIZE;//MAX_JPEG_BUF_SIZE;/*status.bufInfo.minOutBufSize[0];*/

              /* Basic Algorithm process() call */

            

             retVal = IIMGENC1fxns->process((IIMGENC1_Handle)handle,

               (XDM1_BufDesc *)&inputBufDesc,

               (XDM1_BufDesc *)&outputBufDesc,

               (IIMGENC1_InArgs *)&inArgs,

               (IIMGENC1_OutArgs *)&outArgs);

 

             if(retVal == XDM_EFAIL)

               {

 

                 LOG_printf(&trace, "\n Process function returned an Error...  ");

                 return  FAILURE; 

                

               }

            

             if (outArgs.currentAU < swAuNum)

             {               

                LOG_printf(&trace, "\n currentAU is less than  the total AuNum  ");

                return  FAILURE;

             }

 

             LOG_printf(&trace, "process cnt(%d)",uwCnt++);

 

            /* DeActivate the Algorithm                */

 

                 handle->fxns->algDeactivate(handle);

 

 

        }

}

 /**********************************************************************************************/