Here are some approximate numbers that Tommy got of RTC current at room temperature. RTC current did not vary significantly between RUN and STOP modes:
Current consumption on RTC with the core powered up to 1.2V was in the 175-177uA range.
Current consumption on RTC with the core powered down to 0V was in the 12-14uA range.
Clarification for the two sets of numbers: