Other Parts Discussed in Thread: CCSTUDIO
Hi, I hit a problem when I use Jpeg library( Build ID: 2.00.002) in my project.
My code is bellow which very simple, I do it as the demo from “dm6446_jpegenc_2_00_002_production\packages\ti\sdo\codecs\jpegenc\app\Client\Test”.
-When I run this task in DSP side without DSPlink environment, the .out file is loaded via emulator from JTAG, the While-loop can run continuously.
-But When I run these code in DSP side with DSPLINK, which means boot from arm and two cores run together, the program crashed after soon. I doubted that maybe the DSPLINK configuration is incorrect in my project. Then I used the dsplink demo from “dsplink_1_30_08_02\packages\dsplink\dsp\src\samples\scale”. I add my code in the function “static Int tskScale()” , before the DSPLINK related code” status2 = TSKSCALE_create (&info);”. It crashed as well. Of course, I have checked the stack size and heap size, and try to enlarge it if it’s too small. Besides, I know the program crashed in "IIMGENC1fxns->process" by invoking the “abort()” function.
This problem has troubled me for several days. I tried almost all ways I can figure out. but nothing changed. Any help would be greatly appreciated. Thanks.
Meisi
ps:The attachment is the image data I uesed in my project.The format is yuv420(352*288,semiplanar format ,luma is planar but,chroma channels are interleaved).
/*********************************************************************************/
#define CIF_HEIGHT 288
#define CIF_HALF_HEIGHT 144
#define CIF_WIDTH 352
#define CIF_IMG_SIZE 101376 //(CIF_HEIGHT * CIF_WIDTH)
#define CIF_HALF_SIZE 50688
#define CIF_YUV420_SIZE 152064 // 10
UINT8 uacImgYUV[CIF_YUV420_SIZE];
UINT8 uacImgOutput[CIF_YUV420_SIZE];
JpegProc()
{
FILE *pFileIn;
int swRtnVal;
UINT8 *pInBuf[3];
Uns uwCnt = 0;
int uwImgLength = 0;
IIMGENC1_Params tGlobalParams;
IIMGENC1_DynamicParams tDynamicParams;
IALG_Handle handle;
IIMGENC1_Fxns *IIMGENC1fxns;
IIMGENC1_Status status;
XDAS_Int32 retVal;
/* Input/Output Buffer Descriptor variables */
XDM1_BufDesc inputBufDesc, outputBufDesc;
IIMGENC1_InArgs inArgs;
IIMGENC1_OutArgs outArgs;
int ii;
int swAuNum;
pFileIn = fopen("C:\\CCStudio_v3.3\\MyProjects\\Data\\yuv420_uvuv.txt","rb");
if (pFileIn != NULL)
{
swRtnVal = fread(uacImgYUV,1,CIF_IMG_SIZE,pFileIn);
if (swRtnVal != CIF_IMG_SIZE)
{
LOG_printf(&trace, "fread failed 1 %d\n",swRtnVal );
}
}
else
{
LOG_printf(&trace, "fopen failed\n" );
}
pInBuf[0] = uacImgYUV;
tGlobalParams.size = sizeof(IIMGENC1_Params);
tGlobalParams.maxHeight =288;
tGlobalParams.maxWidth = 352;
tGlobalParams.maxScans = 0;
tGlobalParams.dataEndianness = XDM_BYTE;
tGlobalParams.forceChromaFormat = XDM_GRAY;//XDM_YUV_420P;
if ((handle = (IALG_Handle)ALG_create (
(IALG_Fxns *) &DMJPGE_TIGEM_IDMJPGE,
(IALG_Handle) NULL,
(IALG_Params *) &tGlobalParams)) == NULL)
{
#ifdef DEBUG_INFO_PRINT
LOG_printf(&trace, "\nFailed to Create Instance... Exiting for this configuration..");
#endif
return FAILURE;
}
status.size = sizeof(IIMGENC1_Status);
inArgs.size = sizeof(IIMGENC1_InArgs);
outArgs.size = sizeof(IIMGENC1_OutArgs);
outArgs.extendedError = 0;
outArgs.bytesGenerated = 0;
outArgs.currentAU = 0;
tDynamicParams.captureWidth = 352;
tDynamicParams.generateHeader = 0;
tDynamicParams.inputChromaFormat = XDM_GRAY;//XDM_YUV_420P;
tDynamicParams.inputHeight = 288;
tDynamicParams.inputWidth = 352;
tDynamicParams.numAU = 0;
tDynamicParams.qValue = 80;
tDynamicParams.size = sizeof(IIMGENC1_DynamicParams);
while(1)
{
/* Activate the Algorithm */
handle->fxns->algActivate(handle);
/* Assigning Algorithm handle fxns field to IIMGdecfxns */
IIMGENC1fxns = (IIMGENC1_Fxns *)handle->fxns ;
/* Optional: Set Run time parameters in the Algorithm via control()*/
retVal = IIMGENC1fxns->control((IIMGENC1_Handle)handle, XDM_SETPARAMS,
(IIMGENC1_DynamicParams *)&tDynamicParams,
(IIMGENC1_Status *)&status);
if(retVal != IALG_EOK || status.extendedError)
{
LOG_printf(&trace, "control failed(%d)",status.extendedError);
return FAILURE;
}
/* Get Buffer information */
retVal = IIMGENC1fxns->control((IIMGENC1_Handle)handle,
XDM_GETBUFINFO,
(IIMGENC1_DynamicParams *)&tDynamicParams,
(IIMGENC1_Status *)&status);
if(retVal != IALG_EOK || status.extendedError)
{
LOG_printf(&trace, "control failed(%d)",status.extendedError);
return FAILURE;
}
swAuNum = status.totalAU;
/*Fill up the buffers as required by algorithm */
inputBufDesc.numBufs = status.bufInfo.minNumInBufs ;
inputBufDesc.descs[0].buf = (XDAS_Int8 *)pInBuf[0];
inputBufDesc.descs[0].bufSize = status.bufInfo.minInBufSize[0];
for(ii=0; ii< (status.bufInfo.minNumInBufs - 1);ii++ )
{
inputBufDesc.descs[ii+1].buf = (XDAS_Int8 *)pInBuf[ii + 1];
inputBufDesc.descs[ii +1].bufSize =
status.bufInfo.minInBufSize[ii +1];
}
outputBufDesc.numBufs = status.bufInfo.minNumOutBufs ;
outputBufDesc.descs[0].buf =(XDAS_Int8 *) uacImgOutput;
outputBufDesc.descs[0].bufSize = CIF_YUV420_SIZE;//MAX_JPEG_BUF_SIZE;/*status.bufInfo.minOutBufSize[0];*/
/* Basic Algorithm process() call */
retVal = IIMGENC1fxns->process((IIMGENC1_Handle)handle,
(XDM1_BufDesc *)&inputBufDesc,
(XDM1_BufDesc *)&outputBufDesc,
(IIMGENC1_InArgs *)&inArgs,
(IIMGENC1_OutArgs *)&outArgs);
if(retVal == XDM_EFAIL)
{
LOG_printf(&trace, "\n Process function returned an Error... ");
return FAILURE;
}
if (outArgs.currentAU < swAuNum)
{
LOG_printf(&trace, "\n currentAU is less than the total AuNum ");
return FAILURE;
}
LOG_printf(&trace, "process cnt(%d)",uwCnt++);
/* DeActivate the Algorithm */
handle->fxns->algDeactivate(handle);
}
}
/**********************************************************************************************/