This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x PRU pin assignment for PROFINET

Guru 15520 points

Other Parts Discussed in Thread: AM3357, TLK105L

Hi,

I have questions about AM335x PRU-ICSS.

My customer are developing PROFINET using AM3357 ZCZ package.

They are connectin two TLK105L to AM335x PRU by MII. And they assigned the pins for PRU as attached file.

They don't know the reason, but only PRU0 MII0 are not working(not communicating).

They are using pr1_mii0_rxd[3:0] signal for mii0_rxd[3:0](Internal signal of PRU-ICSS),

so that they set pin_mux_sel[0] to "0" as AM335x TRM(spruh73l) page.204 Figure 4-3.

 

Q1. Is there any register to be configured for pin setup?

Q2. As pin assignment of attached file, they configured PRU col and crs signal.

Is the PROFINET communication possible while supporting COL and CRS signals of PRU according to the attached file(pin assignment)?

Q3. I want to know which PRU pins are needed for PROFINET.

Is there any manual or list about pin assignment of PRU for PROFINET?

AM335x PRU pin Assignment for PROFINET.xlsx

best regards,

g.f.