Hi All,
I was looking for a step-by-step tutorial that can guide me on how
to work directly on the hardware level of the OMAP3530 processor on a beagleboard.
I intend to do video capturing and processing as quickly as
possible(from a cold start). TI claims that OMAP3530
can capture images in 1/10th of a second. I would like to make use of
this instead of waiting for the Linux OS to boot(which currently is
less than 3 secs).
It would be of great help if somebody can provide a tutorial to work
with code composer studio(CCS) and beagleboard.
I am also wondering if I can download binary from CCS to nand flash on beagleboard and later execute it.
Thanks in advance,
Vinay.