Other Parts Discussed in Thread: CCSTUDIO
I have specified a path in the Build Options , DspBiosBuilder tab, but when I try to open the DSP/BIOS config GUI, i get an a prompt looking for a path name for tci fiel search. If i dont give it one, it goes on to show me this as below. No where in the reported path or environment is the path i specifiy. I have CCS 3.3 3.3.82.13
I have checked that my path in the build options tab has forward slashes.
I get this problem inconsistently among projects.
any ideas?
js: "C:/CCStudio_v3.3/bios_5_33_04/xdctools/include/utils.tci", line 510: exception from uncaught JavaScript throw: Error: Can't find import file: 'dsplink-omap3530-base.tci' (not found along 'C:/SVN/dsp/Build/;;C:/CCStudio_v3.3/bios_5_33_04/packages;C:\CCStudio_v3.3\bios_5_33_04\xdctools/include;C:\CCStudio_v3.3\bios_5_33_04\xdctools/packages')
"./RDC_DSP_App.tcf", line 21
"./<stdin>", line 4
Correct any script errors in C:/SVN/Red/trunk/sw/dsmc1/brain_module/dsp/Build/RDC_DSP_App.tcf
using the Configuration Tool or a text editor, if necessary.
TConf initialization arguments:
-e environment['config.importPath']='C:/CCStudio_v3.3/bios_5_33_04/packages' -e environment['config.scriptName']='RDC_DSP_App.tcf'