This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VIN Issue from FPGA

Hi ,

We are using DM8148 on out custom board. DM8148 is interfaced with FPGA. VIN is connected to FPGA. FPGA is feeding data on VIN. We are using DVRRDK 04_01_00_02

1) There is a color bar generation module in the FPGA which generates 1080p30 YUV422 16bit Embedded sync. I am able to capture this data and display on the HDMI. 

2) There is a External video decoder chip ADV7842 interfaced to FPGA. When FPGA is feeding the data taken from ADV7842 to DM8148 I am unable to capture the data and display. From the study we understood that ADV7842 is driving 16bit YUV 422 compliance (BTU656). From the DVRRDK API GUIDE,it supports 16 bit- BT1120 standard. Does n't DM8148 or DVRRDK supports  16bit YUV 422 compliance (BTU656) ??. If yes, how to configure capture in BTU656 mode. I am pasting the DVRRDK API content which tells 16Bit -BT1120.

SYSTEM_CAPT_VIDEO_IF_MODE_8BIT 

Embedded sync mode: 8bit - BT656 standard

SYSTEM_CAPT_VIDEO_IF_MODE_16BIT 

Embedded sync mode: 16bit - BT1120 standard

SYSTEM_CAPT_VIDEO_IF_MODE_24BIT 

Embedded sync mode: 24bit

SYSTEM_CAPT_VIDEO_IF_MODE_MAX 

Maximum modes 

Thanks and Regards,

K.Pranay