This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UBI error: ubi_init: cannot attach mtd1

Hi,

I am working on EVMK2H and my evm is not booting linux from ubifs. After u-boot these messages are printed. I think my nand flash is corrupted. How can I solve this?

Creating 1 MTD partitions on "nand0":
0x000000180000-0x000020000000 : "mtd=2"
UBI: attaching mtd1 to ubi0
UBI: physical eraseblock size:   131072 bytes (128 KiB)
UBI: logical eraseblock size:    126976 bytes
UBI: smallest flash I/O unit:    2048
UBI: VID header offset:          2048 (aligned 2048)
UBI: data offset:                4096
UBI error: ubi_read_volume_table: the layout volume was not found
UBI error: ubi_init: cannot attach mtd1
UBI error: ubi_init: UBI error: cannot initialize UBI, error -22
UBI init error 22
UBIFS error (pid 0): ubifs_get_sb: cannot open "ubi:boot", error -19
UBIFS error (pid 0): ubifs_mount: Error reading superblock on volume 'ubi:boot'
Regards
Rao