Other Parts Discussed in Thread: AM3358
Hi,
I use AM3358 Starter Kit.
When I run StarterWare example project neonVFPBenchmark, the result in the console window is:
The compiler and linker options are coming from the StarterWare(I do not modify it at all).
Do you see the NEON instructions from this project?
Here is the compiler options:
-mv7A8 --code_state=32 --abi=eabi -me -O2 --opt_for_speed=2 --include_path="C:/ti/ccsv5/tools/compiler/arm_5.1.1/include" --include_path="../../../../../../../include" --include_path="../../../../../../../include/hw" --include_path="../../../../../../../include/armv7a/am335x" --include_path="../../../../../../../include/armv7a" --gcc --diag_warning=225 --display_error_number --diag_wrap=off --neon
This is the linker options:
-mv7A8 --code_state=32 --abi=eabi -me -O2 --opt_for_speed=2 --gcc --diag_warning=225 --display_error_number --diag_wrap=off --neon -z -m"neonVFPBenchmark.map" -i"C:/ti/ccsv5/tools/compiler/arm_5.1.1/lib" -i"C:/ti/ccsv5/tools/compiler/arm_5.1.1/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="neonVFPBenchmark_linkInfo.xml" --ram_model