This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do I must program DM8148 C674x when I do not use DSP algorithm?

The application is this:

I need to use  DaVinci Video Processorsto capture DVI Port :1600X1200 pixels @60Hz;I need to commpact the video with H.264,then stored it throug SATA II Port.

The FAE recommended to use DM8148,But I am not familar with DSP program,I do not need any intelligence algorithm.Do I must program  DM8148 C674x when I do not use DSP algorithm?Or I just do not care aboat the DSP program?

  • Hi ,
    It depends on the usecase you are based on.
    I guess you are going to modify the existing usecase in DVRRDK to get your own usecase.
    So If you dont need DSP, just go through the usecase code and make sure all the links which may use DSP are removed.
    Then there should be no problem.

    BR,
    Eason