This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Am3352 Fast External Booting problem in u-boot(SDK7.0)

Hi,

   I use Fast External Booting from norflash(non-muxed).Hardware is done in accordance with non-muxed.  I just modify the norflah code,

here below are the norflash entry for pin mux and nor configuration,

#if defined(CONFIG_NOR) && !defined(CONFIG_NOR_BOOT)
static struct module_pin_mux bone_norcape_pin_mux[] = {
{OFFSET(lcd_data0), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A0 */
{OFFSET(lcd_data1), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A1 */
{OFFSET(lcd_data2), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A2 */
{OFFSET(lcd_data3), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A3 */
{OFFSET(lcd_data4), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A4 */
{OFFSET(lcd_data5), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A5 */
{OFFSET(lcd_data6), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A6 */
{OFFSET(lcd_data7), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A7 */
{OFFSET(lcd_vsync), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A8 */
{OFFSET(lcd_hsync), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A9 */
{OFFSET(lcd_pclk), MODE(1)| PULLUDEN | RXACTIVE}, /* NOR_A10 */
{OFFSET(lcd_ac_bias_en), MODE(1)| PULLUDEN | RXACTIVE}, /* NOR_A11 */
{OFFSET(lcd_data8), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A12 */
{OFFSET(lcd_data9), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A13 */
{OFFSET(lcd_data10), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A14 */
{OFFSET(lcd_data11), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A15 */
{OFFSET(gpmc_a0), MODE(4) | PULLUDEN | RXACTIVE}, /* NOR_A16 */
{OFFSET(gpmc_a1), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A17 */
{OFFSET(gpmc_a2), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A18 */
{OFFSET(gpmc_a3), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A19 */
{OFFSET(gpmc_a4), MODE(4) | PULLUDEN | RXACTIVE}, /* NOR_A20 */
{OFFSET(gpmc_a5), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A21 */
{OFFSET(gpmc_a6), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A22 */
{OFFSET(gpmc_a7), MODE(1) | PULLUDEN | RXACTIVE}, /* NOR_A23 */

{OFFSET(gpmc_ad0), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD0 */
{OFFSET(gpmc_ad1), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD1 */
{OFFSET(gpmc_ad2), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD2 */
{OFFSET(gpmc_ad3), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD3 */
{OFFSET(gpmc_ad4), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD4 */
{OFFSET(gpmc_ad5), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD5 */
{OFFSET(gpmc_ad6), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD6 */
{OFFSET(gpmc_ad7), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD7 */
{OFFSET(gpmc_ad8), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD8 */
{OFFSET(gpmc_ad9), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD9 */
{OFFSET(gpmc_ad10), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD10 */
{OFFSET(gpmc_ad11), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD11 */
{OFFSET(gpmc_ad12), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD12 */
{OFFSET(gpmc_ad13), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD13 */
{OFFSET(gpmc_ad14), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD14 */
{OFFSET(gpmc_ad15), MODE(0) | PULLUDEN | RXACTIVE}, /* NOR_AD15 */

{OFFSET(gpmc_csn0), (MODE(0) | PULLUDEN) | RXACTIVE}, /* NOR_CE */
//{OFFSET(gpmc_advn_ale), (MODE(0) | PULLUDEN) | RXACTIVE}, /* NOR_ADVN_ALE */
{OFFSET(gpmc_oen_ren), (MODE(0) | PULLUDEN | RXACTIVE)},/* NOR_OE */
//{OFFSET(gpmc_be0n_cle), (MODE(0) | PULLUDEN | RXACTIVE)},/* NOR_BE0N_CLE */
{OFFSET(gpmc_wen), (MODE(0) | PULLUDEN | RXACTIVE)}, /* NOR_WEN */
//{OFFSET(gpmc_wait0), (MODE(0) | RXACTIVE | PULLUDEN)}, /* NOR WAIT */
{-1},
};
#endif

#define STNOR_GPMC_CONFIG1 0x00001000
#define STNOR_GPMC_CONFIG2 0x00101000
#define STNOR_GPMC_CONFIG3 0x00030301
#define STNOR_GPMC_CONFIG4 0x10041004
#define STNOR_GPMC_CONFIG5 0x000C1010
#define STNOR_GPMC_CONFIG6 0x08070280
#define STNOR_GPMC_CONFIG7 0x00000E48

I successfully download u-boot.bin  in norflash. then change sysboot.

When single step debug to function of save_boot_params,then  the program jumps to 0x0800000C,This address seems to enter  function of  _software_interrupt. it stop here so that  Fast External Booting fail. I find that address of save_boot_params is 0x08001B2C,It is beyond the 4K range. Please let me know is anything wrong i'm doing? what's wrong with it ?

here below are the save_boot_params code.

reset:
bl save_boot_params

ENTRY(save_boot_params)
ldr r1, =OMAP_SRAM_SCRATCH_BOOT_PARAMS
str r0, [r1]
bx lr
ENDPROC(save_boot_params)