Other Parts Discussed in Thread: TMS320TCI6614
1) Is there any clock that need to be provided to EVM when EVM – RF Board is connected via optical cable
2) Are there any registers in PHY and AIF2 registers that can be monitored to check the AIF2 link status ie to know if sync is achieved or not. In case there are errors observed in AIF2 registers or PHY, then what does it correspond to and how can the info be used to understand why the sync is not happening or resolve the sync
3) Assume in EVM-RF Board combination, EVM is always CPRI master and is the default config – can this be confirmed
4) How to set the default CPRI link rate to 2.46 Gbps?