This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet reception hang up after conducted immunity test

Hi,

We are performing the conducted immunity test (EN-6100-4-6) in a AM335 with an external Micrel KSZ8081 PHY and using the kernel 3.14.26. Some times after performing this test, the Ethernet reception doesn't work until we restart it using "ifdown eth0; ifup eth0". Do you know what's happening?

Also we detected a strange value in "Rx Align/Code Errors": This value have an high increase just before the reception hang up.

root@circutor:~# ethtool -S eth0 | grep "Errors"
     Rx CRC Errors: 1
     Rx Align/Code Errors: 613

Any help would be most welcome!