This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

7 inch LCD doesn't work in Beaglebone black



Hi,

I am porting 7 inch LCD cape onto Beaglebone black refernecing below.  

processors.wiki.ti.com/.../Processor_SDK_Linux_LCDC

I am using "Processor SDK Linux 1.00.00.00".

But LCD never worked and no fbdev was created with messages below.

[    1.495347] tilcdc 4830e000.lcdc: no encoders/connectors found
[    1.501588] tilcdc 4830e000.lcdc: failed to initialize mode setting

I had copied then compiled dts file from am335x-boneblack-lcd7.zip

Is there anything needed in addition to dtb file to enable LCD interface?

Any help would be greatly appreciated.

Best regards,

Luke