This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why OMAP-L137 is slower than DSK6713 for my project

Other Parts Discussed in Thread: OMAP-L137

I am doing performance test on OMAP-L137 and DSK6713. the codebase is the same, it  is only c source code, it contains alot of function call, if statements and switch statements, but doesn't do many DSP calculations. The optimization are set to  level 3  for both DSP boards.

the clock for OMAP-L137 is 300MHz, and DSK6713 is 225MHz. I measure the performance by switching LED, and the JTAG is connected to the boards when measuring. The result is:

9us for one loop on DSK6713

28us for one loop on OMAP-L137

the DSK6713 it is about 3x faster then OMAP-L137 for my code. I what to know whether it is OK or not.