Other Parts Discussed in Thread: TPS65218
Hi,
There is a question about specifications of I2C of AM437x.
With the data sheet of both devices of AM437x and TPS65218, it is following mentions as specifications of I2C.
AM437x:VOL(max)=0.45V
TPS65218:VIL(max)=0.4V
In this case I think that SDA and the case that I cannot receive transmission data from AM437x in the TPS65218 side normally together SCL are possible.
Is there a problem?
It is like VOL(max)=0.4V when I watch the specifications of other devices supporting I2C.
Is it the mistake of the data sheet of AM437x?
Best Regards,
Shigehiro Tsuda