This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIRTOS HTTP Web Server

hi,
How can I create the http server dynamic manner, ie without the XGCONF?

I mean how can I activate the http service by creating dynamic task ...

TI-RTOS - 2.10.01.38

Micro: TM4C129ENCPD...

regards

Aquino

  • Hi Aquino,

    You can use the NDK's C runtime configuration APIs to add the HTTP server to the NDK.

    I would recommend the following method to get the code for this:

    1. Use a temporary project (e.g. tcpEcho) and update it to add the HTTP server via XGCONF.

    2. Build the project

    3. The necessary C configuration code to create the HTTP server will be generated from the XGCONF configuration during the project's build.

    4. Look at the generated C file to see the code you need to add.  For example:


    Please refer to the NDK API Guide, Appendix G for more details on the legacy runtime configuration APIs.

    Steve

  • hi Steven Connell Thank you for your response.

    regards
    Aquino