This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713 HPI Port

I have been working on the HPI port of C6713 device. I like to connect a tac line signal to one of the HPI port (J1). 

So can i know if i can directly solder the wire to por or should i use any external device to connect the tac line wire.

If i need to use external device, what device should i be using.