Hello everyone,
(target is C6678, compiler 7.4.11, NDK 2_24_01_13)
When I use the NDK I'm running out of space in L2 memory (512 Ko).
I've put some sections in DDR3 to save space but it impacts performance (ethernet + in general signal processing).
Can you help me find out which sections is it safe (low impact) to put in DDR3 and which one are important to put in L2 ?
SECTION L2 or DDR3
.text L2
.const DDR3 ?
stacks L2
switch L2
bss L2
neardata L2
rodata L2
fardata L2
vecs L2
cio L2
far DDR3 ?
.resmgr_memregion L2 ?
.resmgr_pa L2 ?
resmgr_handles L2 ?
.netctrl L2 ?
nimu_eth_ll2 L2 ?
cppi L2 ?
system_heap DDR3 ?
stk DDR3 ?
qmss DDR3 ?
drv_cppi DDR3 ?
drv_pa DDR3?
drv_qmss DDR3 ?
platform_lib DDR3 ?
os DDR3 ?
nettool DDR3 ?
Thank you,
Clement