This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 MAC address change.

Hi. I want to change MAC address in Client demo program. I tried to change it via registers:

volatile UINT32 *MACID_1 = (UINT32 *) 0x02620110;
    volatile UINT32 *MACID_2 = (UINT32 *) 0x02620114;
   /* To Unlock */
    (*(unsigned int*)(0x02620000 + 0x0038)) = (0x83E70B13);
    (*(unsigned int*)(0x02620000 + 0x003C)) = (0x95A4F1E0);


    *MACID_1 = 0xCCDDEEFF;
    *MACID_2 = 0x0000AABB;
    platform_get_emac_info(0, &emac);

But it didn't change.

I want in my project use the IP Stack from Client project, but i need to change MAC address.

How can i do that?

Thanks.