This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

To send and to recieve ethernet frames. TMDSEVM6670L



Hello again. 

I'm using the 2.21.02.43 NDK and 2.01.02.06 MCSDK with an client example. 

I want to send and recieve the raw ethernet packet, using only the C instructions, but i can't find any appropriate function, that could help me. Also, i can't watch port i should listen to, to intercept those packets. I've not changed the "evmc6670 client" example, but i want to add the "send" and "recieve" functions.