Hi,
In the hyperlink example, it is mentioned that in token exchange, a token (sequence number) is passed symmetrically between the two devices. Does symmetrically here mean that core x on the first board only exchanges tokens with core x on the second board ? where x= 0,1,2,...7.
If that is the case, what needs to be changed in the example to have, for instance, core 0 on one board exchanging tokens with core 1 on the second board (i.e. having different cores on different boards exchanging tokens)?
Thanks!