Hi.
I tried running the HyperLink example program available with the PDK packages on a c66 EVM. I uncommented the necessary line to enable loopback mode, linked all necessary files, and ran it on the board.
However, the program does not seem to progress past the initialization stage. Console output is as follows:
*****************************************************
[C66xx_0] Version #: 0x01000105; string HYPLNK LLD Revision: 01.00.01.05:Mar 3 2014:19:49:43
About to do system setup (PLL, PSC, and DDR)
********************************************************
Could someone please tell me why the program is not progressing past system setup?
Thanks.