Hi,
I am currently working on the TCI6614 device and want to boot up the ARM core through CCS v5.5. the GEL file that came in the board CD is not able to get the ARM running but works fine with DSP.
Is there another gel file for ARM or will the same gel file work with some changes?
My steps:
>> Make a target configuration with connector as 560v2 USB mezzanine and board as TCI6614
>> Launch the target config
>> OUTPUT panel shows that the DSPs are up but gives the error "Can't Connect to device" for ARM
Thanks
Raunak