This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[MCSDK-VIDEO] sv04 build and tftp server

Hi,

Just a quick question.
I'm now trying MCSDK-VIDEO (MCSDK-VIDEO 02_01_00_08) demo:

http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.1_CODEC_TEST_FW_User_Guide

It seems sv04 has been built successfully by following "Make Instructions" described in the above wiki.
I found the executable and readme_sv04.txt in dsp/mkrel/sv04.
But I saw the following in the generated readme file:

============================

DSP_VERSION 2.1.0.8
BUILD NAME sv04
RTP YES
CPU Type C6416
Build Type HDCT
H264BP_DEC NO
H264MP_DEC NO
H264HP_DEC NO
MPEG2MP_DEC NO
MPEG4_DEC NO
H263_DEC NO
H264BP_ENC NO
MPEG4_ENC NO
H263_ENC NO
Build ID 0
Built At (MM/DD/YYYY HH:MM:SS) 06/22/2015 11:08:22 GMT

============================

As you see, CPU Type looks C6416 and dec/enc features looks disabled... Is this expected ?
Please note I wants to run sv04 on C6678EVM with TFTP server.

Also, the above wiki shows the link to TFTP server for windows environment, but the link looks dead... Any comments ?

Best Regards,
Naoki