Other Parts Discussed in Thread: SYSBIOS
hello
I use ...
1. vision_sdk_02_05
2. ccs5.0
now...I got a problem about memory allocate
Q1: I try to use malloc to create memory space... the size may be under 96*160*9(int)
and the program can be compiled and run...but it has a message "ti.sysbios.heaps.HeapMem: line 307: ti.sysbios.heaps.HeapMem: line 307: out of memory: handle=0x970ee298, size=552968"
Q2: I try to create more heap size for it...in C:\VISION_SDK_02_05_00_00\ti_components\drivers\starterware_01_02_04_05\examples\sbl_multicore_mbx\tda2x\lnk_dsp1
""DDR3_DSP1_HEAP : org = 0x85500000, len = 0x00500000"" to change "len"
but it doesnt work!!!
Could you please to tell me what I can do for "malloc" in c66 dsp?
Thanks a lot.
B.R
by Alice