Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO
Dear all,
I'm trying to boot the EVMOMAP-L137 from the SPI flash memory.
I have follow the steps in here: processors.wiki.ti.com/.../Boot_Images_for_OMAP-L137
There is a sample code that implements a blinker: the DSP enable the ARM, then the ARM turns on and off some leds in the board.
Now my problem: I added a few lines to the DSP code in order to control the UART. The code is presented as follows:
#include "device.h"
#include "evmomapl137_uart.h"
#define KICK0Ra *(unsigned int*)(SYS_BASE + 0x038)
#define KICK1Ra *(unsigned int*)(SYS_BASE + 0x03c)
void main(void)
{
UART_Handle uart0;
// Open Permissions to SYSCFG Registers (Not required for PG2.0 silicon and above)
KICK0Ra = 0x83e70b13;
KICK1Ra = 0x95A4F1E0;
DEVICE_enable_ARM();
uart0 = EVMOMAPL137_UART_open( 2, 1248 ); // This work for baud=9600. baud*24000000*13/(16*150000000)
while(1){
while( EVMOMAPL137_UART_xmtReady( uart0 ) ); // Wait for uart_tx ready
EVMOMAPL137_UART_putChar( uart0, 'A' ); // Write 1 byte
}
}
e2e.ti.com/.../964737
e2e.ti.com/.../103027
e2e.ti.com/.../412104
So, I just enable the ARM, then I send continuously 'A' through the serial port. When I lunch the project from ccs3.3 everything works ok: I see the leds blinking and receive continuously 'A' in my PC.
However, when the code is downloaded to the SPI flash, and the OMAP-L137 boots from it, I can see the leds blinking, but I don't receive anything in my PC (nothing comes out from the UART, I checked it with an oscilloscope).
This is the DSP linker.cmd file (I have just added the path to evmomapl137bsl.lib with respect to the original file):
-lrts64plus.lib
-l C:\CCStudio_v3.3\boards\evmomapl137_v1\dsp\lib\evmomapl137bsl.lib
-stack 0x00001000 /* Stack Size */
MEMORY
{
L2RAM org=0x80010000 len=0x00010000 /* L2 RAM/Cache */
}
SECTIONS
{
.text > L2RAM
.const > L2RAM
.bss > L2RAM
.far > L2RAM
.switch > L2RAM
.stack > L2RAM
.data > L2RAM
.cinit > L2RAM
.sysmem > L2RAM
.cio > L2RAM
}
This is the ARM linker.cmd file:
/*
* Linker command file
*
*/
-
-stack 0x00000800 /* Stack Size */
-heap 0x00000800 /* Heap Size */
MEMORY
{
ARMRAM: o = 0xFFFF0000 l = 0x00002000
DSPRAM: o = 0x11800000 l = 0x00040000
SHAREDRAM: o = 0x80000000 l = 0x00020000
SDRAM: o = 0xC0000000 l = 0x20000000
}
SECTIONS
{
.bss > SHAREDRAM
.cinit > SHAREDRAM
.cio > SHAREDRAM
.const > SHAREDRAM
.stack > SHAREDRAM
.sysmem > SHAREDRAM
.text > SHAREDRAM
.switch > SHAREDRAM
.far > SHAREDRAM
.test_buf > SDRAM
}
Does anybody have any idea why the code doesn't work when booted from the flash?