I have a DVEVM 6446. How can I flash the entire file system to the board?. Is there any softwares or emulators available for doing this task? . Please help me regarding this
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a DVEVM 6446. How can I flash the entire file system to the board?. Is there any softwares or emulators available for doing this task? . Please help me regarding this
Hi Sid
Thanks for the reply. I want to flash a sample application devolped by me. I have written an application to display an image on the LCD display associated with the board. Now I want to flash that on to the Board . How can I do that?. Can you please help me on that
Hi Vishnu,
What are you using?
Linux or Code Composer Studio?
If using CCS, then you need an emulator.
If using Linux, then you use NFS to mount the uboot, linux kernel and filesystem on DM6446 ,once mounted successfully, you will get a prompt and you can run the program on it. For this you need to give your program path on the prompt.
Regards,
Sid
Hi Sid
I have mounted the application on the NFS and I had run it . In between I m using OpenSuse Linux 11.2. But I want to flash this application on the TI board memory rather than keeping it on the NFS . How can I do that ? Can you give me some idea on that ?
Hi Sid
If you consider the standalone demo,even without connecting the TI board to the PC ,the stand alone demo will work . Like that I need to make my application work on the Ti board , this is my real intention. I m new to this field . Please help me on that. Is there any particular document regarding this.?
I m not using Code Composer Studio.
Hi Vishnu,
If you want to flash the application on TI board memory, then you need to program the FLASH with the application code and bootloader. The processor will then boot from flash and load the contents of the flash in its internal RAM (depending on the size of your application) and run your application. TI has Flash programmer applications like SLH_DM646x.exe and SFH_DM646x.exe which are Serial Flash loading utilities. You will have to dig around for the corresponding commands to program your on-board flash with your application code.
Regards,
Sid
Hi Vishnu,
Yes, the current standalone demo will be erased.
I dont remember exactly, but here are 2 Flash memories on DM6446 EVM with the corresponding flash memory selectable using Boot Options switch. These are the NOR Flash and NAND flash. Check the FLASH which contains the current standalone demo. Maybe you can use other Flash to run your code on startup.
Or there might exist the corresponding Flash file of the standalone demo in the SDK examples/demo codes. You can reprogram the Flash with it and restore the board to its default status.
Regards,
Sid
hi sid
by looking the previous mails i think you can solve my problem what i am facing . actually i am using DM6446EVM board while runing the board without ethernet cable i am not able to run the demo and i get the following messages wile i am booting the board.so, please refer this and give reply
U-Boot 1.1.3 (Dec 4 2006 - 12:05:38) U-Boot code: 81080000 -> 81097628 BSS: -> 810A0018 RAM Configuration: Bank #0: 80000000 256 MB Flash: 16 MB In: serial Out: serial Err: serial ARM Clock :- 297MHz DDR Clock :- 162MHz Hit any key to stop autoboot: 3 2 0 DaVinci EVM # tftp 0x80700000 uImage TFTP from server 10.0.0.2; our IP address is 10.0.0.1 Filename 'uImage'. Load address: 0x80700000 Loading: *################################################################# ################################################################# ################################################################# ################################################################# ########################################### done Bytes transferred = 1551032 (17aab8 hex) DaVinci EVM # boot ## Booting image at 80700000 ... Image Name: Linux-2.6.18_pro500-davinci_evm- Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 1550968 Bytes = 1.5 MB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK OK Starting kernel ... Uncompressing Linux........................................................................................................ done, booting the kernel. Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@localhost.localdomain) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Tue Apr 27 12:04:22 IST 2010 CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177 Machine: DaVinci EVM Memory policy: ECC disabled, Data cache writeback DaVinci DM6443 variant 0x0 CPU0: D VIVT write-back cache CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets Built 1 zonelists. Total pages: 30208 Kernel command line: video=davincifb:vid0=0,2500K:vid1=0,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=ntsc console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/hda1 mem=118M PID hash table entries: 512 (order: 9, 2048 bytes) Clock event device timer0_0 configured with caps set: 03 Console: colour dummy device 80x30 Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 118MB = 118MB total Memory: 116224KB available (2653K code, 527K data, 152K init) Security Framework v1.0.0 initialized Capability LSM initialized Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok DaVinci: 71 gpio irqs WARNING: both IDE and NOR flash are enabled, but share pins. Disable IDE for NOR support. ch0 default output "COMPOSITE", mode "NTSC" MUX: initialized LOEEN MUX: initialized LFLDEN VPBE Encoder Initialized LogicPD encoder initialized SCSI subsystem initialized usbcore: registered new driver usbfs usbcore: registered new driver hub davinci_spi_board_init: NO spi support VFS: Disk quotas dquot_6.5.1 Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) squashfs: version 3.1 (2006/08/19) Phillip Lougher JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc. yaffs Apr 27 2010 12:01:49 Installing. SGI XFS with no debug enabled Initializing Cryptographic API io scheduler noop registered io scheduler anticipatory registered (default) LTT : ltt-facilities init LTT : ltt-facility-core init in kernel davincifb davincifb: dm_osd0_fb: Initial window configuration is invalid. davincifb davincifb: dm_osd0_fb: 720x576x16@0,0 with framebuffer size 2025KB davincifb davincifb: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 2500KB davincifb davincifb: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB davincifb davincifb: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 2500KB davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownership of OSD window. DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a 16550A RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize Linux video capture interface: v2.00 vpfe vpfe.1: DaVinci v4l2 capture driver V1.0 loaded Trying to register davinci display video device. layer=c0ddde00,layer->video_dev=c0dddf60 Trying to register davinci display video device. layer=c0dddc00,layer->video_dev=c0dddd60 davinci_init:DaVinci V4L2 Display Driver V1.0 loaded Davici AEW Driver cannot be loaded VIDEO PORT is not enabledData Flow path from CCDC is disabled Davinci AF driver cannot be loaded VIDEO PORT is not enabled CCDC needs to be configured<6>i2c /dev entries driver Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2 ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx MUX: initialized HDIREN MUX: initialized ATAEN ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio hda: TOSHIBA MK4032GAX, ATA DISK drive ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22 hda: max request size: 512KiB hda: 78140160 sectors (40007 MB), CHS=16383/255/63, UDMA(66) hda: cache flushes supported hda: hda1 hda2 Initializing USB Mass Storage driver... usbcore: registered new driver usb-storage USB Mass Storage support registered. usbcore: registered new driver usbhid drivers/usb/input/hid-core.c: v2.6:USB HID core driver musb_hdrc: version 6.0, cppi-dma, host, debug=0 musb_hdrc musb_hdrc: No DMA interrupt line musb_hdrc: USB Host mode controller at c785e000 using DMA, IRQ 12 musb_hdrc musb_hdrc: MUSB HDRC host driver musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1 usb usb1: configuration #1 chosen from 1 choice hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected mice: PS/2 mouse device common for all mice rtc_davinci_evm rtc_davinci_evm: rtc intf: proc rtc_davinci_evm rtc_davinci_evm: rtc intf: dev (254:0) rtc_davinci_evm rtc_davinci_evm: rtc core: registered rtc_davinci_evm as rtc0 rtc0: hours 12-23 are misreported as duplicate hours 00-11 davinci-mmc davinci-mmc.0: Supporting 4-bit mode davinci-mmc davinci-mmc.0: Using DMA mode Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC). ASoC version 0.13.1 MUX: initialized MCBSP AIC3X Audio Codec 0.1 asoc: aic3x <-> davinci-i2s mapping ok ALSA device list: #0: DaVinci EVM (aic3x) Time: timer0_1 clocksource has been installed. Clock event device timer0_0 configured with caps set: 08 Switched to high resolution mode on CPU 0 rtc_davinci_evm rtc_davinci_evm: setting the system clock to 2004-02-01 12:01:58 (1075636918) kjournald starting. Commit interval 5 seconds EXT3 FS on hda1, internal journal EXT3-fs: recovery complete. EXT3-fs: mounted filesystem with ordered data mode. VFS: Mounted root (ext3 filesystem). Freeing init memory: 152K INIT: version 2.86 booting [31m*[39;49m udev requires hotplug support, not started. [31mfailed![39;49m Activating swap...done. Remounting root filesystem...done. Calculating module dependencies Loading modules: Checking all file systems: fsck fsck 1.40 (29-Jun-2007) Mounting local filesystems: mount nothing was mounted Setting up networking .... /etc/network/options is deprecated. Setting up IP spoofing protection: FAILED. Starting network interfaces: No usable address families found. socket: No such file or directory Failed to bring up lo. done. Kernel hotplug support not enabled. Starting portmap daemon.... Cleaning: /tmp /var/lock /var/run done. Setting pseudo-terminal access permissions...done. Updating /etc/motd...done. INIT: Entering runlevel: 3 Starting system log daemon: syslogd klogd. Starting NFS common utilities: statd. Starting internet superserver: inetd. Starting OpenBSD Secure Shell server: sshd. CMEMK module: built on May 26 2009 at 09:30:32 Reference Linux version 2.6.18 File /db/atree/library/trees/linuxdemos/linuxdemos-d28x/imports/DEMO_common/linuxutils_2_23_01/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c ioremap_nocache(0x87600000, 10485760)=0xc8000000 allocated heap buffer 0xc8000000 of size 0x2c000 cmem initialized 5 pools between 0x87600000 and 0x88000000 dsplinkk: no version for "struct_module" found: kernel tainted. DSPLINK Module (1.61.03) created on Date: May 26 2009 Time: 09:35:23 Starting web server ... thttpd MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921) (none) login: root Last login: Sun Feb 1 12:31:40 2004 on console Linux (none) 2.6.18_pro500-davinci_evm-arm_v5t_le #1 PREEMPT Tue Apr 27 12:04:22 IST 2010 armv5tejl GNU/Linux Welcome to MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921). root@(none):~# ls root@(none):~# cd / root@(none):/# ls bin dev home lost+found mnt proc sbin sys usr boot etc lib media opt root srv tmp var root@(none):/# cd /opt/dvsdk/dm6446/ root@(none):/opt/dvsdk/dm6446# ./loadmodules.sh insmod: error inserting 'cmemk.ko': -1 File exists insmod: error inserting 'dsplinkk.ko': -1 File exists root@(none):/opt/dvsdk/dm6446# ./decode -v data/videos/davincieffect_ntsc.m2v Decode demo started. Error: Failed to create attribute window device Error: Failed to create UI root@(none):/opt/dvsdk/dm6446# davinci_
thanks & regards
ramki