Hi
Sorry if I am in the wrong forum,
I am trying to implement ETHERNET/IP communication on one ICEV2 Board, basing myself on the SDK EIP example.
I have just bought a license to use the EIP stack from molex on which the example is based. But the example's precompiled lib does things that the stack I bought is unable to do, namely there seems to be a whole ACD api that I can't find in the source code from Molex or in the source code of the SDK .
Here are all the functions that I'm missing :
Description Resource Path Location Type
unresolved symbol ACD_Exit, first referenced in ./eip_main.obj octiv_sysbios C/C++ Problem
unresolved symbol ACD_IncTick, first referenced in ./user_acd_ndk.obj octiv_sysbios C/C++ Problem
unresolved symbol ACD_Init, first referenced in ./eip_main.obj octiv_sysbios C/C++ Problem
unresolved symbol ACD_Link, first referenced in ./user_acd_ndk.obj octiv_sysbios C/C++ Problem
unresolved symbol ACD_RcvArpFrame, first referenced in ./user_acd_ndk.obj octiv_sysbios C/C++ Problem
unresolved symbol ACD_Start, first referenced in ./user_acd_ndk.obj octiv_sysbios C/C++ Problem
unresolved symbol ACD_Stop, first referenced in ./user_acd_ndk.obj octiv_sysbios C/C++ Problem
Could anyone point me in the right direction ?
Best regards
Adrien