This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Examples of L2 Cache Configured as SRAM on AM437x

I'm having difficulty using the L2 cache as RAM on the AM437x. My understanding is the device powers up with L2 cache disabled and the RAM is powered and clocked. I've defined section in the memory but I'm unable to load code through the emulator to those locations. I'm also not able to access it manually through the emulator.


Are there any simple examples available? Hints?


Best regards,

Neil