Other Parts Discussed in Thread: AM3517
Hello,
I am using AM35x-OMAP35x-PSP-SDK-03.00.00.05 sdk with my AM3517 EVM board. When I connect a usb mouse, I am getting:
hub 1-0:1.0: Cannot enable port 1. Maybe the USB cable is bad?
hub 1-0:1.0: Cannot enable port 1. Maybe the USB cable is bad?
hub 1-0:1.0: Cannot enable port 1. Maybe the USB cable is bad?
hub 1-0:1.0: Cannot enable port 1. Maybe the USB cable is bad?
hub 1-0:1.0: unable to enumerate USB device on port 1
errors, and mouse is not recognized. I ve tried various kinds of mouses(including very standart 2 button mouses), none worked.
But I can connect usb flash disk on the board, No problem with it.
To solve the problem, I tried disabling EHCI and enabling OHCI on kernel. But this time, the board also didn't recognize any plug-in action.
What is the problem with USB connection?
Thanks in advance.
Yigit