We are using LTE PHY (LWP 1410) provided by TI as part of our LTE program, involving integration with a external RRH. The build folder name is 6614_phy_main_20140617_1904_RF_TDD_HW5_UIA1 and binary file version is phy_main_20140617_1904_RF_TDD.out.
We are unable to establish CPRI sync between BBM and RRH, which is not SCBP.
Going through the Release Notes provided with the binary, we noted that the Compilation Settings of HLTC binaries is with "HW platform: Appleton (Cfg_HW_PLATFORM = 5)". This HW Platform Setting corresponds to "case of TCI6614 on the Appleton EVM board with SCBP Relay RF (all revisions), as mentioned in section 6.2.1. It also notes that choice of Cfg_HW_PLATFORM affects the active CPRI link used by PHY.
Is the LTE L1 binary provided to us with the same setting mentioned above? If yes, would it be expected to work with a non-SCBP RRH or would the HW Platform relevant in our case need to be "1" (case of TCI6614 on the Appleton EVM board with baseband (all revisions)).
Regards,
Amit