I am running the audio filter demo on the VC5505 eZdsp. When I plug in a headphone completely to the HP OUT jack I only get mono (Lt out). If I pull the connector out of the jack about 1/8 inch, then I get stereo. I am using AA handout headphone with standard 3.5mm connector. Works fine for PC out. Only with eZdsp stick do I see a problem. Has anyone else experienced this? Any suggestions on what might be causing this?
Thanks.