Greetings!
Circuit configuration:
I have designed a DSP 6713B board that use TPS70345 regulator for reset and 1.2V and 3.3V for the processor. TPS70345 output 22 uF (for 3.3V) and 47 uF (for 1.2 V) are low ESR capacitors as per recommendations.
It has 1M x 32 bit FLASH connected to CE1. HD[3:4] are pulled up through 33R resistors.
I have managed to program FLASH with valid code through XDS510USB emulator.
Problem:
Whenever the board is powered up after a while, CE1 doesn't appear (doesn't turn low indicating FLASH reading for 1 K primary boot loading) and hence the system doesn't boot from FLASH. However, if I turn it OFF and then turn ON IMMEDIATELY, the CE1 does appear and the system boots normally.
What could be the problem with system not booting when powered up after a while?