Other Parts Discussed in Thread: 66AK2E05
Hi all,
We are developing a Custom Hardware Development based on TI 66AK2E05 Keystone II processor,
There is Microcontroller support in 66AK2E05 (Stellaris LM3S2D93).
In our Custom Hardware development we have all the interfaces and support that 66AK2E05 EVK has except one that we don't have Microcontroller support
. Instead the Hardware itself will do all the operations that Micro controller does in 66AK2E05 in our board
We need to remove all the Hardware and Software dependencies that the Processor have on Microcontroller and Vice versa on u-boot and Linux Kernel
EVMK2E_Technical_Reference_Manual.pdf
In the Reference manual, in Figure 2.6: EVMK2E BMC Connections
In the connections between BMC and 66AK2E05 SoC, we like to know what UART0_TX, I2C(SDA0 and SCL0) does
What purpose does these pins possess and what operation does three pin does in uboot and Linux kernel
We need to isolate these in Code and remove the dependency that these pins possess with the Micro controller.
Also I like to know whether those I2C interface is slave or master
Please help with this.
Thanks & Regards,
Sarjoon.