Other Parts Discussed in Thread: UNIFLASH, AM3358, FLASHTOOL
Hi,
I followed the Sitara Uniflash Quick Start Guide to flash android Image into my board witch has an AM3358 MPU. after i have did all the steps and click
the Start Flashing button, the Progress value stay at 0% for a long time and the other instance of USB RNDIS driver haven't appear. bellow is the log of
opendhcp and opentftp:
[07-Jul-15 15:14:43] Logging: All
[07-Jul-15 15:14:43] Open DHCP Server Version 1.59 Windows Build 1036 Starting...
[07-Jul-15 15:14:43] DHCP Range: 192.168.2.2-192.168.2.254/255.255.255.0
[07-Jul-15 15:14:43] Server Name: 2014-20140719FL
[07-Jul-15 15:14:43] Detecting Static Interfaces..
[07-Jul-15 15:14:43] Lease Status URL: http://127.0.0.1:6789
[07-Jul-15 15:14:43] Listening On: 192.168.2.1
[07-Jul-15 15:14:48] BOOTPREQUEST for d0:5f:b8:fb:e8:b3 () from interface 192.168.2.1 received
[07-Jul-15 15:14:48] BOOTP Host d0:5f:b8:fb:e8:b3 (Hostd05fb8fbe8b3) allotted 192.168.2.3
[07-Jul-15 15:14:43] Open TFTP Server MultiThreaded Version 1.64 Windows Built 2001 Starting..
[07-Jul-15 15:14:43] starting TFTP service
[07-Jul-15 15:14:43] alias / is mapped to C:\AM335x_Flashtool\images\
[07-Jul-15 15:14:43] permitted clients: all
[07-Jul-15 15:14:43] server port range: all
[07-Jul-15 15:14:43] max blksize: 65464
[07-Jul-15 15:14:43] default blksize: 512
[07-Jul-15 15:14:43] default timeout: 3
[07-Jul-15 15:14:43] file read allowed: Yes
[07-Jul-15 15:14:43] file create allowed: No
[07-Jul-15 15:14:43] file overwrite allowed: No
[07-Jul-15 15:14:43] thread pool size: 1
[07-Jul-15 15:14:43] Listening On: 192.168.2.1:69
[07-Jul-15 15:14:48] Client 192.168.2.3:1234 C:\AM335x_Flashtool\images\u-boot-spl-restore.bin, 208 Blocks Served
PS: i use a USB TO UART uint to see the log of flash, but i get nothing in the window of serial port debug tool,why? (I connect the USB TO UART uint with uart0)
Please help me to solve the mentioned problem above, thank you.