Since there are some limitations with booting using 4GB eMMC under MMC0 management as described
within 26.1.7.5.2 from the AM335X TRM Rev. L
Will this option work ????
1. if we will have MMC0 that manages both eMMC and NAND
2. Partition with MLO and u-boot.img is stored within NAND
3. Partition with targetNFS is stored on 4GB eMMC
Booting will start from NAND and continue with targetNFS portion from within eMMC-4GB
or this option is also forbidden under section 26.1.7.5.2
Maybe somebody tried it and can share the results...
Thanks,
Naum Grutman