Hi,
I am using the TMS320C6A8167 integra board and CCSv5.5 to connect to the ARM core. I want to run a simple socket program that gets packets from the Ethernet and stores it in memory I have included the socket.h and init.h files from the ndk folder of MCSDK, but I am getting errors about UINT8/16/32 being not defined and HANDLE not defined etc. my code:
#include<stdio.h>
#include<string.h>
#include<stdlib.h>
#include<inet.h>
#include<socket.h>
#include<ctype.h>
#define BUFLEN 1500 //Max length of buffer
#define PORT 8080 //The port on which to listen for incoming data
int counter =0;
void die(char *s)
{
perror(s);
exit(1);
}
int main(int argc , char**argv)
{
struct sockaddr_in server_addr, client_addr;
int sockfd , i, slen = sizeof(client_addr) , recv_len ;
char buf[BUFLEN];
if ((sockfd=socket(AF_INET, SOCK_DGRAM, IPPROTO_UDP)) == -1)
{
die("socket");
}
memset((char *) &server_addr, 0, sizeof(server_addr)); // replaces the client addr to 0
server_addr.sin_family = AF_INET;
server_addr.sin_port = htons(PORT);
server_addr.sin_addr.s_addr = htonl(INADDR_ANY);
client_addr.sin_family = AF_INET;
if( bind(sockfd,(struct sockaddr*)&server_addr, sizeof(server_addr) ) == -1)
{
die("bind");
}
while(1)
{
//printf("Waiting for data...");
fflush(stdout);
if ((recv_len = recvfrom(sockfd, buf, BUFLEN, 0, (struct sockaddr *) &client_addr, &slen)) == -1) // read datagram from server socket
{
die("recvfrom()");
}
counter++;
//sendto(sockfd, buf, recv_len, 0, (struct sockaddr*)&client_addr, slen) ;
//printf("Received packet from %s:%d\n", inet_ntoa(client_addr.sin_addr), ntohs(client_addr.sin_port));
printf("Data: %s\n" , buf);
printf("counter: %d\n",counter);
}
}
the following screen shot gives the errors:
are there some example projects for arm where I can see how to use the header files.
Thanks
Raunak