Other Parts Discussed in Thread: DM3730
Hi All,
I am working on the DM3730 core Varicite board. Android Gingerbread is ported on the board. When kernel booted up USB-OTG is working in client mode, after system is reboots, at U-boot USB-OTG is not working. When the user issued the adb-reboot command, kernel reboot the system by the WARM RESET by the PRM_RSTCTRL.RST_GS soft reset. I changed the reset to Cold reset RST_DPLL3, so it is working fine.
Is there is any USB-OTG issue with the Global warm reset?
BR,
Kishore