This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3 xloader with HWECC

Hi,

 

CSST is a good tool to flash to NAND thru USB boot mode. However it uses HW ECC as the ECC format. Flashing x-loader with HW ECC is needed since the BootROM uses that ECC format. However when flashing u-boot with CSST, the out of the box xloader cannot read u-boot from flash, because it expects SW ECC. Does anyone have an x-loader that supports HW ECC? I am currently working on patching in HW ECC into the x-loader.

 

Regards,

--Gunter