Other Parts Discussed in Thread: TPS65930
Hi
I am working on custom board having OMAP 3530 and TPS65930 as the PMIC. We are using RTC of TPS65930 and it is powered by coin cell battery. It’s observed that the RTC resets its date and time to 2000-01-01 00:00:00 occasionally upon board power cycle and the voltage at the coin cell battery looks good and it is around 3.1V.
Please find the log of one such instance
/***************************************************************************/
twl4030_rtc twl4030_rtc: setting the system clock to 2010-04-28 17:20:47 (1272475247)
After power cycle
twl4030_rtc twl4030_rtc: setting the system clock to 2000-01-01 00:00:00 (946684800)
/***************************************************************************/
Please let us know if this is known issue with TPS family and any workaround available.
With Regards
Srinath