Other Parts Discussed in Thread: ADS1274
Hi,
I am using EVMC6678L EVM to read data from ADC. I want to use ADS1274 from TI.
ADC chip has TDM and SPI interfaces. But the problem is that SPI interface is only 24bit.
As I know, C6678 only support 8 or 16 bit SPI.
Can I use ADS1274 for EVMC6678L EVM?
Actually, ADS 1274 datasheet has a example hardware design. The example design is to connect ADS 1274 to TMS320VC5509.
But this example is using Multi channel BSP for connection. I think 6678 has no McBSP and only have TSIP.
I think TSIP is different from McBSP. Am I correct?
Thanks in advance.
Baeyoung