Other Parts Discussed in Thread: AM3354
now i connect am3354 with a fpga by gpmc,i have configured the gpmc Synchronous burst mode,and i have want to read 4kb datas from fpga by edma ,from oscilloscope i can see the wave form is is similar to Figure 7-45.but i can only get the 4th data in the edma destination address,the ahead 3 datas are all lost,who can tell me what can i do to solve the problem?thankyou very much.
the follow is my configuration:
1,gpmc configuration:
val = GPMC_CONFIG1_READMULTIPLE_SUPP;
val |= GPMC_CONFIG1_WRAPBURST_SUPP;
val |= GPMC_CONFIG1_READTYPE_SYNC;
val |= GPMC_CONFIG1_WRITETYPE_SYNC;
val |= GPMC_CONFIG1_CLKACTIVATIONTIME(1);
val |= GPMC_CONFIG1_PAGE_LEN(0);
val |= GPMC_CONFIG1_DEVICESIZE_16;
val |= GPMC_CONFIG1_DEVICETYPE_NOR;
gpmc_cs_write_reg(GPMC_FPGA_CS, GPMC_CS_CONFIG1, val);
2,edma configuration
edma_r_base = kmalloc(2 * 2048,GFP_KERNEL);
edma_r_phy_base = dma_map_single(NULL,edma_r_base,2048*2,DMA_FROM_DEVICE);
if (dma_mapping_error(NULL, edma_r_phy_base)) {
myprintk("fail to dma_map_single");
return -EIO;
}
edma_set_src (dma_ch, (unsigned short *)fpga_phy_base + args, INCR, W16BIT);
edma_set_dest (dma_ch, (unsigned short *)edma_r_phy_base, INCR, W16BIT);
edma_set_src_index (dma_ch, 0, 0); // use fifo, set zero
edma_set_dest_index (dma_ch, 2,2048 * 2 ); // A mode
edma_set_transfer_params (dma_ch, 2, 2048, 1, 1, ABSYNC);
edma_read_slot (dma_ch, ¶m_set);
param_set.opt |= (1 << ITCINTEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch));
edma_write_slot (dma_ch, ¶m_set);
3,start edma
init_completion(&my_completion);
ret = edma_start(dma_ch);//开始传输
if(ret != 0)
{
printk("fail to edma_start");
}
wait_for_completion(&my_completion);
edma_stop(dma_ch);